2. Newlec | News

News | Rexel Extends Its Newlec Range With New Products

Rexel Extends Its Newlec Range With New Products

Electrical distributor Rexel has extended its Newlec Industrial controls offer to supply a more comprehensive range to customers.

The expansion of so many product lines makes the Newlec Industrial controls range one of the largest own brand offers on the market.

Within the newly expanded offer are extensions to existing product offers, such as additional operating voltages for contactors and relays. Contactors are now available with 24VAC coils, a more common and safer control voltage for motor control panels, adding to the 230VAC and 400VAC coils already available.

Further voltages have been added to the range of industrial plug in relay products, now available in 12VDC, 24VDC, 24VAC, 110VAC and 230VAC. In two, three and four pole. Further additions are added such as slim Din Rail relays for space saving applications and one and two pole interface relays. There is also a range of solid-state relays suitable for more arduous conditions and higher switching rates.

An expansion of the successful pushbutton range has been made to include new two position selector switches and key switches. A robust range of pushbutton pendants for crane applications have also been added. These are available as two, three, four and five button stations in one and two speeds.

With a look towards current and future developments, a 22mm Ethernet and USB outlets have been made available in a push button housing. This is a significant development removing costly downtime caused by having to open the control panel door for diagnostics. The new products allow users to simply plug in a device to access data and work in a safe environment.

Mark McCall, Product Manager at Rexel, said: “We’re extremely excited by these recent developments to our product offering. This extension means our own brand offer is one of the largest available on the market. This is significant for Rexel and our customers as we are enabling contractors to improve their own work and customer offering by accessing more quality products at their convenience.

“This new range highlights our ambition to progress and support our customers, for example this is the first time we have offered an enclosed switch fuse range up to 400A, this complements the already successful enclosed switch disconnect range which has been further developed to include switches up to 400A. The new products are available in branch or for same day or next day delivery. And for customers requiring more technical support, we will also have the support of the Rexel Industrial Solution branches.”

For more information on Rexel’s services and solutions visit: www.rexel.co.uk

› Back to news
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
Note on the processing of your data collected on this website in the USA by Google, Facebook, LinkedIn, Twitter,Youtube: by clicking on "Accept all", you also consent in accordance with Art. 49 para. 1 sentence 1 lit. a GDPR that your data will be processed in the USA. The US is assessed by the European Court of Justice as a country with an inadequate level of data protection according to EU standards. In particular, there is a risk that your data may be processed by US authorities for control and monitoring purposes, possibly even without the possibility of redress. If you click on "Only accept essential cookies", the transmission described above will not take place.